8/16/2019 4:31 PM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Dear Martin, The first item I saw is the computer name does not follow the rules of PCS 7. See attached. But I guess it might not be the reason. 1. Please check the physical connection and make sure you can ping each other. 2. Make sure you have assign OS server, right click on Sposa OS-> Assign OS server. 3. Make sure the target path is correct \\Computer Name\Automation projects is shared and accessible by the engineering station. 4. Make sure you can access the target computer and not block by any hardening policy of the computer. Hope it helps. AttachmentRules of Computer Name.pdf (205 Downloads) |
Last edited by: JazTai at: 08/16/2019 16:31:29Please give me 5 stars Rating if my post is helpful for you. :) |
|
8/17/2019 3:48 AM | |
Joined: 10/26/2017 Last visit: 4/4/2022 Posts: 3 Rating: (0) |
Hi JazTai, I have try to re-setup, but the problem still exist, do you have experience to make this SPOSA working before? I have follow the openpcs7 guideline setup, but unfortunately cannot get the expected result i want. 1. Please check the physical connection and make sure you can ping each other. Answer: Yes, window command ping have done. 2. Make sure you have assign OS server, right click on Sposa OS-> Assign OS server. Answer: Yes, primary and standby server have assigned. 3. Make sure the target path is correct \\Computer Name\Automation projects is shared and accessible by the engineering station. Answer: Yes, share drive with this folder also accessible 4. Make sure you can access the target computer and not block by any hardening policy of the computer. Answer: Yes, new PC no have any hardening policy setup. Attachment44444703_openpcs_7_station_opc-clients_en.pdf (203 Downloads) |
8/17/2019 9:47 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
I attached with my project configuration for your comparison. Hope it helps you little bit. What you could check also is the PCStation name, please configure your computer name into it. And please make sure your Computer name is configured in the Host file. You must be able to ping with your Computer name but not IP address. Before doing all these, go to computer - > simatic shell -> right click at the top -> settings -> choose your terminal bus IP address/network card. make sure the system is using the correct terminal bus to do download into OPC station. AttachmentOPC_Configuration.pdf (243 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on