7/31/2017 7:41 AM | |
Joined: 12/28/2015 Last visit: 1/24/2024 Posts: 256 Rating: (26) |
Yes, you can do it via script and write the user authentification into a txt file or an sql database. |
8/3/2017 9:56 AM | |
Joined: 8/3/2009 Last visit: 6/5/2024 Posts: 12991 Rating: (1659)
|
Hello Summer88 I´m not sure but I Think its a function that creates an operator Message in the normal alarm Logging and ther is also a system Block "comment". So if you enter the Comment in the Dialog box then it will be written in the comment field in this operator Message. Bye Murof |
If this Information really helps, you could use the Rate function |
|
8/4/2017 3:42 PM | |
Joined: 2/5/2013 Last visit: 3/26/2024 Posts: 287 Rating: (5) |
Thanks for answer, I've just tried tia v14 sp1 on windows10 2016 enterprise, it just keep crashing. Will try with UDP2... Just to know, is this production ready or better going on with windows7 and tiav13? |
Follow us on