1/28/2011 1:20 PM | |
Joined: 10/7/2005 Last visit: 10/8/2024 Posts: 3024 Rating: (1054)
|
Hello simaticfan79 let me start by welcoming you to this Forum followed by some good news answer to your questions which is: You can in principle use/operate any DP Slave on the 95U's DP Master port and the FAQ "DP slaves on AG95 DP master" also verifies this. What this FAQ unfortunately neglegts totell you is that if you operate a DP Slave on a 95U that is a.) capable of issuing more than 32 Bytes of Diagnostic data and b.) does so for whatever reasons will cause aCPU stop! COM Profibus V5.x checks the DP Slave GSD file for this and will thus NOT allow you to configure DP Slaves fora 95U DP Master that are capable of sending more than 32 Bytes of Diagnostic data (older versions of COM Profibus do NOT check for this, see also HERE for more on this). What I suggest you do is this: Decide on a range of DP Slaves that you would behappy to use asa replacement for the WAGO DP Slaves. Download their GSD files, do a test config of them in COM Profibus V5.x (which will tell you if can or can not use them) and then decide which ones to order. If you do not have COM Profibus V5.x, you can alternatively open each GSD with a text Editor and search for the "Max_Diag_Data_Len" entry in them, any one with a value bigger than 32 is off limits. Alternatively, consider replacing the 95U with an S7 first and later replace theWAGO I/O's with now any DP Slave that you can think off. You will find some more useful info in the ET 200 Distributed I/O System with IM 308-C and S5-95U manual I hope this helps Edit:You will find some more useful info in the ET 200 Distributed I/O System with IM 308-C and S5-95U manual |
Last edited by: fritz at: 1/28/2011 1:55 PMAdded S5 ET200 manual link Cheers |
|
This contribution was helpful to1 thankful Users |
2/4/2011 12:48 PM | |
Joined: 1/4/2011 Last visit: 10/6/2024 Posts: 22 Rating: (0) |
Thank You all for Your help! In the near future S5 will be migrated to S7 for sure. But now we have a lot of problems with WAGO I/O therefore WAGO has to be replaced first immediately. CPU works great for now (knock,knock). After distributed I/O migration we would have more time to prepare for S5 to S7 migration. As I see it on this link ET200S in not on the list. Does that mean that ET200S 100% DOES NOT work with S5-95U? ET200S is similar size as WAGO and it would be best solution for replacement... So as I see it ET200M is the only solution... Am I right? What would be the reason that ET200S does not work with S5-95U and that ET200M does? Where is the difference? Thank You! |
2/4/2011 1:27 PM | |
Joined: 10/7/2005 Last visit: 10/8/2024 Posts: 3024 Rating: (1054)
|
Hello simaticfan79 thereason for the ET200S NOT being in THISlist is that the entry dates back to 1996 and the ET200S did NOT exist back then. Please read my previous entry again carefully and do the checksthat I suggest you doto determine if you can use a particular DP Slave on a 95U (i.e. do a test config im COM Profibus or search the GSD forthe "Max_Diag_Data_Len" entry). Bottom line: Any DP Slave that is capable of issuing more than 32 Bytes of Diagnostic data is off limits for your 95U and while I haven't check all available ET200M or S, you'' find that most (or all) recent oneswill NOT be useable as they have a "Max_Diag_Data_Len" of greater than 32. I hope this helps |
Cheers |
|
2/5/2011 11:45 AM | |
Joined: 10/7/2005 Last visit: 10/8/2024 Posts: 3024 Rating: (1054)
|
Same advise as before dear simaticfan79: Please read my previous entry carefully and especially the link to THISFAQ in it. |
Cheers |
|
Follow us on