11/20/2007 10:33 AM | |
Posts: 8 Rating: (0) |
Hi, dchartier thanks! i knowit is means that u talk to me.but i don't know it is means in this Segment 2.Would u tell me?...... Best Regards light |
11/20/2007 2:16 PM | |
Posts: 8 Rating: (0) |
Hi, dchartier, thanks so much! this system include 135U CPU 928 and use IM308B connect some ET200U , the program i show u is L2 net diagnostic program,the page addressis be use,but i don't know "127" and "0" means. :C DB 253MONITORING BUSDB :L KB 48PAGENO. :T OY 255 :L KY 127, 0 :T OW 252 :L OY 252 :T DR 19DIAGNOSIS:OUTLINE0-15 :L OY 253 :T DL 19DIAGNOSIS:OUTLINE0-15 BEST REGARDS LIGHT |
11/21/2007 5:16 AM | |
Posts: 8 Rating: (0) |
Hi, dchartier, thanks! You know "L KY (station number), (code) Load station number: 3 to 125 andcode: 0 to 7" but at here "127" is what means? "3 to 125"?? BR light |
11/22/2007 3:07 PM | |
Posts: 8 Rating: (0) |
Hi, everyone, anybody know "L KY (station number), (code) Load station number: 3 to 125 andcode: 0 to 7" but at here "127" is what means? "3 to 125"?? BR light |
12/19/2007 6:00 PM | |
Joined: 9/27/2006 Last visit: 7/29/2024 Posts: 12272 Rating: (2676) |
Hello light; Sorry it took so long to see your last question; I hopethe answer can still be of help. Prtofibus-DP reserves address 127 for broadcast (from a master to all connected slaves) and for multicast (master to a specified group of slaves). The slaves do not answer when recieving indata on address 127. There is not much information on broadcast for the S5 CPUs. Here is an extract from a manual on the Profibus interface of the S5-95U: Prerequisites for multicasting: • You must assign the same receive SAP in the DB1s of all receiving stations ( section 8.3). • You must enter the global address for multicasting "127" in byte 6 of the request header. http://support.automation.siemens.com/WW/view/en/1091429 Here is a link that explains how it can be used in S7 PLCs: the connection s via FDL, and can only be implemented through Profibus CPs: http://support.automation.siemens.com/WW/view/en/20987711 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 19.12.2007 18:02 |
|
12/21/2007 10:43 AM | |
Posts: 8 Rating: (0) |
thank you so much! BR light |
Follow us on