5/25/2007 11:50 AM | |
Posts: 17 Rating: (0) |
Hello, I have a project with fallow configuration: - 1 simatic S7 station CPU 315 – redundant (whit 2 CPU 315-2DP) - 1 PC HMI Station with Wincc Flexible - 2 small Allen Bradley PLC ControlLogix Is possible communication between PC HMI Station with Wincc Flexible and CPU 315-2DP via MPI and make redundancy on some MPI connection. I send you my project in support question (bat not in forum > 1M)(probably the hardware configuration is not 100% correctly because I do not receive for now software for redundancy). The project have 3 parts vest_pac.zip.part01, vest_pac.zip.part02 and vest_pac.zip.part03 I send 01 and 02 now and 03 in next replay. If the hardware configuration is not OK, please you ken make modification for my. Please help my. AttachmentVest_p_1.zip (232 Downloads) |
5/26/2007 6:08 AM | |
Posts: 15 Rating: (0) |
Hi mr july It is possible redundancy with MPI cable and that MPI cable should be in Y cable, so that two of them connect to CPU, and othe point is connectect to PC. so i have modified the HW configuration. AttachmentVest_p_1.zip (224 Downloads) |
5/30/2007 7:44 AM | |
Posts: 17 Rating: (0) |
Thank you very mach for your prompt answer. |
Follow us on