4/24/2011 12:21 PM | |||||||||
Joined: 8/5/2009 Last visit: 7/4/2022 Posts: 156 Rating: (7) |
Hi, Is it possible to configure an S7 315 PN DP V3.2 6ES7315-2EH14-0AB0 with S7 V5.4 SP4 or SP5 ??? I read something about it: https://support.automation.siemens.com/WW/llisapi.dll/46119963?func=ll&objId=46119963&objAction=csView&nodeid0=33516848&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=treecontent&prodLstObjId=36816516&prodLstStart=41&prodLstSort=MLFBSTR ------------------------------------------------------- In the case of a spare part repelacement:
Configuration with older software versions:
Configuration with the new firmware: ------------------------------------------------------- Its not very clear? |
||||||||
4/24/2011 7:52 PM | |
Joined: 8/5/2009 Last visit: 7/4/2022 Posts: 156 Rating: (7) |
so it is possible to send a project with 315 2EH14 v3.1 (configured in hardware config) to an CPU 315 2EH14 V3.2 (Hardware config and programm) With Step7 V5.4 SP5 , and this will work. i don´t need the new features , the most important is that it works |
Last edited by: dendhondt at: 4/24/2011 7:58 PMLast edited by: dendhondt at: 4/24/2011 7:56 PM |
|
4/24/2011 8:01 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating: (1181) |
Exactly.If the new functions are not required, you can configure the module in STEP 7 as predecessor (FW V3.1) with the latter's scope of functions. Best regards, Hristo Mihalev |
5/5/2011 7:32 PM | |
Joined: 8/5/2009 Last visit: 7/4/2022 Posts: 156 Rating: (7) |
I just tested the configuration S7 V5.4 SP5 with latest hardware updates S7 315-2 PN/DP V 3.2.3 It works fine Thanks for the help Jurgen, |
This contribution was helpful to1 thankful Users |
5/5/2011 8:29 PM | |
Posts: 947 Rating: (45) |
for support new function need Step 7 5.5. |
9/10/2012 10:57 AM | |
Posts: 1 Rating: (0) |
Hello, I have the same problem to do the HW configuration of that CPU. I have ST V5.4 and i can't add the CPU in my HW configuration. How can i do to solve this problem? Would it be possible to send me a HW configuration with that CPU ? Thank you in advance, Best Regards |
9/18/2012 5:52 PM | |
Joined: 8/5/2009 Last visit: 7/4/2022 Posts: 156 Rating: (7) |
In your hardware configuration the highest version of this CPU is V3.1 In step7 V5.4 you need to configure this CPU (V3.2.xxx) as V3.1 and this wil work fine, only the new functions will not work |
Follow us on