10/17/2023 3:43 PM | |
Joined: 10/17/2023 Last visit: 10/17/2023 Posts: 1 Rating: (0) |
This is the seventh machine in the line with the same program, hardware config, and chassis. The module behaves as if it is okay in the hardware config but the SF led is it on the module and the CPU. I've swapped cards, and tried various other things. I believe event 8 is the one causing the issue. I am using type J thermocouples and only the first two channels. Any ideas? More information can be provided if needed. ------------------------------------------------------------------------------------------ AttachmentDiagnose.txt (397 Downloads) |
Last edited by: Jen_Moderator at: 10/18/2023 09:21:55New subject after splitting |
|
Follow us on