5/2/2008 8:26 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (318) |
Hi, Are there connections opened and not used, like the Wireless communication... If not then I recomended to deinstall all the software from Siemens, see the FAQ: How can you completely uninstall STEP 7 including all the software packages? When this is done, then only install STEP7 V5.4 SP3.1 and check if it is better, when not then there is something wrong in Windows XP Professional..... Please use then the restore CD's that coming with the FieldPG.... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on