12/13/2023 2:59 PM | |
Joined: 5/30/2022 Last visit: 9/17/2024 Posts: 578 Rating: (95) |
Hi Pandiani, The build you have indicated is Windows Pro 22H2, so there are no compatibility problems, in the forum we can not help you, so I recommend you to open a Support Request for Siemens to evaluate the log and the project. AttachmentMicrosoft-Windows-10_es_2023-12-13.xlsx (252 Downloads) |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to1 thankful Users |
12/13/2023 3:37 PM | |
Joined: 10/31/2005 Last visit: 9/4/2024 Posts: 366 Rating: (31) |
Thank you, I'll open the request, just as I suspected I'd have to. Thanks for the help! |
7/18/2024 12:02 PM | |
Joined: 9/6/2022 Last visit: 7/18/2024 Posts: 3 Rating: (0) |
Did you manage to find what is the issue ? |
7/25/2024 7:44 AM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13713 Rating: (1728)
|
Hello przygoda If you have a similar problem, you can send us a few more details about your system, used Versions and perhaps a screenshot... or if it occurs only with a specific project try to clear the IM Folder (LINK). It nothing helps, open a Service Request at Siemens Support. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on