11/26/2022 8:56 PM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452) |
Hi k_lamar, as you can find at the delivery release SIMATIC WinCC V18, there is no new dedicated RT Advanced version and also no new device versions for Comfort and Basic panels. It seems that it was not taken into account that when using V18 without previous versions on the computer, the images should be installable. I hope, Siemens will find a solution soon. For the meanwhile try to get the images from a computer with an installed V17. Kind regards |
12/11/2022 8:23 PM | |
Joined: 1/21/2013 Last visit: 5/20/2024 Posts: 2798 Rating: (452) |
Hi, in the meanwhile the DVD "SIMATIC WinCC Legacy Panel Images V18" was published. This setup allows the installation of the V17, Update 5 version of the panel images for the older panels. Kind regards |
6/11/2023 4:46 PM | |
Joined: 3/25/2015 Last visit: 5/15/2024 Posts: 63 Rating: (2) |
Hello. I'm back here because I have a KTP1200 Basic in my V18 project. I've selected 17.0.0.0 as runtime version and obviously I'm missing the panel image. Just for clarification: Do I have to download DVD 4 (Legacy) from this link to make it work? and then upgrade it with v17 upd6 from this link? If yes, this is absolutely madness. Legacy panel images DVD is 7.5Gb and Upd6 is another >2Gb download and install. Why do I have to stick with older versions to be able to download the single panel image? Please make single downloads for all panel images also for V18. UPDATE 1: To be able to install the images on Tia Portal V18 I had to download the package 109746530_SIMATIC_WinCC_Panel_Images_V18.exe from this webpage https://support.industry.siemens.com/cs/document/109746530/image-downloads-for-hmi-operator-panels Even then I cannot select the single image that I'm missing. It's a massive 7.22Gb download and installation for a 90Mb panel image!!! UPDATE 2: Maybe I found a workaround. If you download the full package and just extract without installing, there's a folder with a CAB file inside located at "\SIMATIC WinCC Panel Images V18.0\InstData\WinCC-TrC-All\Media" that contains all the legacy panel images for V16-V17. If you extract it, you will find all the images with a long filename with some GUID in it. Just remove the GUID to have the panel image e.g. for KTP1200: KTP1200DP_V17_00_00_05.FWF_58BF8D94_6292_5F7E_B242_2EE927FB1EFD becomes KTP1200DP_V17_00_00_05.FWF Then put this image inside the Transfer folder as long as the corresponding BUILDINFO.TXT file C:\Program Files\Siemens\Automation\Portal V18\Data\Hmi\Transfer\17.0\Images\KTP1200 Still this requires the full package download, but at least you can copy only the image that you need Let me know if this works for you. |
Last edited by: simonspt at: 06/11/2023 16:51:49Last edited by: simonspt at: 06/11/2023 18:07:24Updates 1 & 2 Kind regards |
|
5/7/2024 4:24 PM | |
Joined: 12/8/2013 Last visit: 5/26/2024 Posts: 3 Rating: (0) |
so i found folder path. there is no exe file. this app can install the panel images automatically? |
Follow us on