3/22/2020 4:58 PM | |
Posts: 2 Rating: (0) |
Hello, Since I have almost same 'problem' and I cannot spend 5000 euro for SAPRO... I have my home automation with S7 1214AC/DC/Relay (6ES7214-1BG40-0XB0) with HMI (Proface GP4301). I want to add also Siemens POL 638 since I can use the software for my AHU. Anyway, I would like to have - MODBUS communication between POL and HMI and - PROFINET between HMI and S7 (this is no problem for me) What can I change in POL's data points with Scope tool in order to have communication between POL, HMI and S7? Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/23/2020 12:20:54New subject after splitting |
|
3/22/2020 5:29 PM | |
Joined: 9/27/2006 Last visit: 4/27/2024 Posts: 12257 Rating: (2665) |
Hello Sorin Siman; Communication modules for Siemens Building Technologies (SBT) are a little out of my comfort zone. Although the protocols used (Modbus RTU in the case of the Climatix systems) are basically the same, it seems you require certain downloadable files to setuup the Modbus mapping for a specific project: Siemens District Heating applications for Climatix comprise predefined monitoring and control functions for a particular plant type. Features: • OEM customers receive standard applications as a set of loadable files. They can be loaded in the controller via SD card. • An HMI operator unit allows for assigning inputs and outputs to the respective plant as well as select, configure and parameterize the required functions. The document attached below does mention the POL638, but not the SCOPE software... Hope this helps, Daniel Chartier AttachmentUserGuide_Climatix_ModBus_VariabelLista_eng.pdf (962 Downloads) |
Follow us on