9/27/2013 2:26 PM | |
Posts: 3037 Rating:
|
Hello, Do you write values of tags in a text file? See the following link, you can use it for WinCC TIA Portal too. http://support.automation.siemens.com/WW/view/en/26107211 Tweety |
10/9/2013 3:01 PM | |
Joined: 4/29/2010 Last visit: 4/30/2024 Posts: 1557 Rating:
|
Hello MAIDEL, no your problem isn´t a real problem in this case. For example if you use a normal tag log in WinCC and you log the tags every second to the memory card... the cycle is the same if you use a script or a log in WinCC. You can do this without any problems. The best will be to use a card wich you can get as HMI Accessorie. Because the function is guaranteed and the cards are tested by Siemens. At this faq you can find all released storage media for the SIMATIC panels: Which external storage media can you use with the SIMATIC panels and which memory card interfaces do they have? With best regards |
This contribution was helpful to
1 thankful Users |
Follow us on