6/22/2013 10:20 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Is this the same post? /tf/WW/en/Posts/93218#top |
6/24/2013 7:20 AM | |
Posts: 209 Rating: (2) |
Hi valli, |
6/24/2013 8:23 AM | |
Posts: 262 Rating: (45) |
OK, I shall help you out. Upgrading firmware is a little tricky. You have to upgrade firmware and language pack one by one. make sure your control supply is intact throughout the execution, any interupption in the power supply will result in destroying that unit. refer the link... download the zip file, unzip itfirst. https://support.automation.siemens.com/WW/llisapi.dll?query=Pac3200&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=csius&objaction=cssearch&searchinprim=&nodeid99= Secindly, you have to load powerconfig in your PC from the below link:- https://support.automation.siemens.com/WW/llisapi.dll?query=powerconfig&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx&lang=en&siteid=csius&objaction=cssearch&searchinprim=&nodeid99= DO the IP address of the PAC meter and communicate it locally through an Ethernet cable. Once PAC started communicating with Powerconfig.. follow the below step ( refer pic attached) Device TAB--- Update--- Device Firmware. Please do the factory reset also immdiately, after disconnecting CT/ PT connection. Look friend... I hope your problem will get resolved. AttachmentFirmware_update.pdf (320 Downloads) |
6/24/2013 8:52 AM | |
Posts: 262 Rating: (45) |
Hi, Yes, you have to disconnect the same. Do factory reset and then firmware updation. |
6/30/2013 10:45 PM | |
Joined: 9/1/2005 Last visit: 5/14/2024 Posts: 4101 Rating: (194) |
closed cause question discussed twice. The second thread with the subject Need help with the PAC3200 erroris published within the same conference. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on