3/18/2024 2:29 AM | |
Joined: 12/27/2023 Last visit: 3/18/2024 Posts: 2 Rating: (0) |
Can I ask how you fo that? Attachment I have this to convert so the software starter will accept it... it won't accept text formats any help would be appreciated thanks Rodney ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/18/2024 13:40:37Link to the quoted attachment optimized. Last edited by: Jen_Moderator at: 03/18/2024 13:43:19New subject after splitting |
|
3/18/2024 4:17 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
which error exactly you get? |
3/18/2024 6:14 PM | |
Joined: 6/4/2008 Last visit: 5/1/2024 Posts: 1484 Rating: (322) |
Hi, EASY! simply download the script and follow instructions in this document https://support.industry.siemens.com/cs/ww/en/view/32582476 You MUST change the extension of your text file (or edit the script to search for .txt instead of .dnl filetypes) Preferred: To change the file extension, run a command prompt and type the following in the location where your file is stored ren "9824-0729-91 02 2_11.txt" "9824-0729-91 02 2_11.dnl" OR alternatively, in the scriptfile on line 23 change to the following APP.Tools.FileBrowser.Open(".txt") I have tried both and they work. One notable mention, you need to set the "NEW" drive in Starter to the firmware version of the new device if that wasn't obvious. The "OLD" drive in your example is v2.1 and additionally has a Profibus address of '3' which is the default address anyway. Regards, Graeme |
4/10/2024 12:57 PM | |
Joined: 3/25/2008 Last visit: 5/2/2024 Posts: 183 Rating: (7) |
don't transfer anything, just change the txt extension to dnl |
Follow us on