Industry Online Support
Technical Forum
2/10/2012 2:33 PM | |
Joined: 4/29/2010 Last visit: 4/30/2024 Posts: 1557 Rating: (161)
|
Hello, first of all check your settings and the connection between the panel and the printer. At this entry you can find a list of all released printers and also the settings to connect them to a panel: http://support.automation.siemens.com/WW/view/en/11376409 Settings on the Printer: On the printer, no settings can be made, i.e. all settings are to be made in WinCE (Panel). Settings in WinCE under "Control Panel" --> "Printer": Printer Language --> Epson 9 Paper Orientation --> Portrait The interface has to be set to USB. Cable: This printer is to be connected via a USB cable. best regards |
2/15/2012 3:47 PM | |
Posts: 3037 Rating: (192)
|
Hello, You should print without this PIO software with TP177B about EPSON LX-300. These were not tested. You can see the tested settings in the following link. http://support.automation.siemens.com/WW/view/en/11376409 Tweety |
Follow us on