11/21/2006 9:25 AM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi, I’ am trying to read the motor current through MM440 using USS protocol and PLC 224XP. I’ am reading the parameter [2018, index 1] and getting the exact reading of frequency. Now problem is although I’ am able to read the correct frequency values I’ am unable to read drive current. Even if I put P2019[1]=27, the drive keep displaying values corresponding to frequency in P2018[1], so is USS_rpm_W. I had factory reset the drive but problem remains. Values of the p2012=2 and p2013=127. Any suggestions why its happening so?? Regards, Manmeet Attachmentuss9.pdf (670 Downloads) |
Follow us on