1/31/2018 7:42 AM | |
Joined: 4/28/2015 Last visit: 8/14/2023 Posts: 8 Rating: (0) |
Dear Expert I want to upload the parameters of the SINAMICS drive on the Profibus PLC network via Ethernet using the STARTER (v4.5) software. The CPU used is 412-2 DP (v5.3) and CP is used type 443-1 (v2.1) which supports routing. The inverter unit is SINAMICS G120 with CU240E-2DP firmware control unit (v4.4) I am using SIMATIC S7 (v5.5 + SP2) software installation on a computer with Windows professional 7. I have followed some of the instructions contained in this forum, but I still can not access SINAMICS drives via Ethernet. Note: to upload drive MICROMASTER 440 (v2.1 and v2.1) I have tried and succeeded, Please help me for the problem I am facing, for the supporting picture is in the attachment. Thank you Regard's Mardiono AttachmentSCREEN SHOOT.zip (383 Downloads) |
1/31/2018 7:53 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008) |
Hello, your G120 FW V4.4 doen't support S7-Routing, and your PLC/CP doesn't support data set routing which is used for this G120 FW Version. https://support.industry.siemens.com/cs/ww/en/view/50037141 Update the G120 FW to >4.7 or connect the G120 directly.
Christoph |
This contribution was helpful to1 thankful Users |
1/31/2018 8:10 AM | |
Joined: 4/28/2015 Last visit: 8/14/2023 Posts: 8 Rating: (0) |
Dear sir Thank you for your response. Please info, how to |
Last edited by: AutoGen_846694 at: 1/31/2018 8:11:26 AMLast edited by: Jen_Moderator at: 1/31/2018 8:32:42 AMEdited text for better reading. |
|
1/31/2018 8:23 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008) |
FW Download: The parameters can be stored on memory card before the update, or you upload first the parameters in starter and change the device version after upload in starter and download then to the CU |
2/1/2018 12:49 PM | |
Joined: 4/28/2015 Last visit: 8/14/2023 Posts: 8 Rating: (0) |
thanks for the information |
Follow us on