3/25/2024 1:29 PM | |
Joined: 8/3/2009 Last visit: 6/5/2024 Posts: 12991 Rating: (1658)
|
Hello SiemensForumUserN... Try with a new test project, just with a button for stop runitme -> does this work? If not then I would do a Reset to factory settings: https://support.industry.siemens.com/cs/de/en/view/109821880 Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/26/2024 6:33 AM | |
Joined: 1/21/2013 Last visit: 6/7/2024 Posts: 2861 Rating: (458)
|
Hi MattShire, What you are describing sounds like a crash. This can happen for a number of reasons, including a bug in your project or a bug in the device. You should make sure that you are running the latest image version on your panel. Using the Trace Viewer may also help you find the cause of your problem. However, you will probably find a large number of messages there, and finding the one that describes the cause of your problem is not easy. This is usually something that Siemens does better. So I would recommend to create a support request. Kind regards |
Follow us on