1/19/2021 2:39 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. I was able to access the drives on this machine until recently but our automation vendor has made changes and I was no longer able to open the drives with Starter v. 5.1 - it told me to update to version 5.3. After downloading the files and transferring them to the PG (it is not allowed to go on the internet) I installed Starter v. 5.3 (after first letting it uninstall v. 5.1). After the installation of the first "CD" I could not see any more setup files so I tried opening the project with the drives again but now I am getting a lot of error messages. What do I need to install to be able to open the drives again and check the parameters and alarms / alarm history? AttachmentFA2 Starter A.zip (598 Downloads) |
1/20/2021 9:02 AM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Thanks again ChristophD, Please also look at the screenshots. I thought I marked everything for installation when I installed it - I have just both searched in the installation files and started a new installation but I do not see any CFC?
AttachmentFA2 Starter B.zip (583 Downloads) |
1/20/2021 9:04 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008) |
if you start cfc then a setup pop up or not? |
1/20/2021 9:22 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008) |
from the cfc directory you see on the one screenshot? "CFC" |
1/20/2021 9:35 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating: (3008) |
go inside the folder insdata/cfc of the install data |
Follow us on