4/27/2023 12:24 PM | |
Joined: 5/19/2010 Last visit: 3/3/2024 Posts: 6 Rating:
|
Hi All, I am also facing similer problem when I migrated project from WinCC flexible 2007 to WinCC Flexible 2008SP3, the migration done without error but during compile face 20 errors, I checked the objects listed in error list, the one tag/Object is displayed or used on multiple screens, data type is also correct and match with symbol list. Can someone guide! ------------------------------------------------------------------------------------------ Attachment2023-04-27 17_22_59-Windows 7 - VMware Workstation 17 Player (Non-commercial use only).jpg (388 Downloads) |
Last edited by: Jen_Moderator at: 04/28/2023 06:48:51New subject after splitting Rizwan Tahir |
|
4/28/2023 7:38 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating:
|
have you also check the setting/property Appereance of the objects? |
5/26/2023 10:23 AM | |
Joined: 8/3/2009 Last visit: 8/15/2024 Posts: 13561 Rating:
|
Hello Tahir EE What i mean was if you have installed the latest Upd for 2008 SP3 before doing the migration? https://support.industry.siemens.com/cs/ww/en/view/58860033 Bye Murof |
If this Information really helps, you could use the Rate function |
|
5/27/2023 5:32 PM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating:
|
Hi, What appeared to you if you clicked on one line of these error messages? It should go to the object and the wrong property setting. And you can compare between this setting and the old setting of the project before migration. Please do it and tell us what appeared to you? |
Ayman Elotaify |
|
Follow us on