12/31/2016 9:15 AM | |
Posts: 116 Rating: (2) |
Hello, We have OP17 connected to CPU S7-300 For a certain tag Z31 Initial MAX value :10 Low value:1 Initial counter set point :20 I opened these data blocks for OP17 Protool program and found the set point is larger than max limit How that? This is a remark and OP17 works good without any problem. Kindly find the attached file. AttachmentDB.zip (430 Downloads) |
12/31/2016 12:11 PM | |
Posts: 116 Rating: (2) |
Hello, Yes these variables used in OP program. I do not know why these variables as in this figure in the program? In OP also I noticed these variables scaled. |
Follow us on