7/10/2023 10:13 AM | |
Joined: 9/23/2005 Last visit: 1/15/2025 Posts: 4393 Rating: (1463)
|
Hi As from TIA V18 up2, it is possible to get / set the S7-1x00 CPUs by WinCC Unified system tags. As from the read me of the up2 in SIOS (https://support.industry.siemens.com/cs/br/pt/view/109817218/en): “... The operating state of an S7-1200/1500 PLC can be read and set via system variables.
The tags are available if a connection to a PLC of the type S7-1200/1500 is configured. The tags are available as of version 18.0.0.2. If the version of a device is changed to an older version, these tags are no longer available. If the connection is removed or the connection type is changed, the tags are removed. This functionality replaces the system functions "SetPlcMode" and "GetPlcMode". ...“ TIPs:
Project AttachmentProject4.zip (732 Downloads) |
Last edited by: Jen_Moderator at: 07/11/2023 07:06:05Text formatting optimized. Denilson Pegaia |
|
This contribution was helpful to3 thankful Users |
Follow us on