工业业务领域支持中心
Technical Forum
6/28/2012 11:13 PM | |
Joined: 9/27/2006 Last visit: 6/14/2024 Posts: 12260 Rating: (2671) |
Hello Aphale;
The support site has a few FAQs on ETU testing for the Sentron ACBs, for example: 3WL9111-0AT44-0AA0 Circuit Breaker Test Device for overcurrent release ETU 15B to ETU 76B 3WL ETU: Internal self-test of overcurrent tripping function does not work Look for more posts using the Search box on the right, with stings such as "ETU testing", "Sentron 3WL"...
I have used Profibus-DP with the Sentron 3VL/3WL ACBs, with good results. But there are many other ways to communicate with the Sentron breakers, as can be seen in this collection of manuals: http://support.automation.siemens.com/WW/view/en/53422640/130000 For more specific details on Profibus exchanges, have a look at this thread: Sentron VL - COM10 Communication
As can be seen in this link, Switch ES was not free, but it is being replaced by a free software: Switch ES Software all variants “Switch ES Power is not available for free download, it can be ordered by using order-no. 3SZ2311-0CC10-0YA0.For the future it shall be replaced by free software powerconfig” Download: Update version powerconfig V2.3 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/29/2012 1:04 AMLast edited by: dchartier at: 6/28/2012 11:21 PMLast edited by: dchartier at: 6/28/2012 11:19 PM |
|
This contribution was helpful to1 thankful Users |
6/29/2012 6:33 AM | |
Posts: 15 Rating: (0) |
Thank you very much Mr.Daniel. Iappreciate your way of explaining things in a detailed &simple way. |
Follow us on