3/6/2007 5:11 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, attached the pin assignment for the SMC30, as you can see on the X521 terminal the A+, A-, B+, B- tracks (in case of unipolar signals A+ and B+, the negated signals all to the ground!) must be connected, in case of zero pulse R+, R- as well. On the X531 terminal the supply (P_Encoder, M_Encoder) must be connected, and in case of temperature evaluation temp+ and temp-. Regards, TechTeam AttachmentSMC30_X521_X531.pdf (3617 Downloads) |
With best regards, |
|
This contribution was helpful to2 thankful Users |
3/6/2016 6:48 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, Please refer the attached sheet of X520 - encoder interface pin configuration. ( I presume encoder is connected to X620). Have you checked your encoder pin details? Is it with track R & R*? Please refer the attached sheet of F31117 for connections of jumper for track R & R*. HTH AttachmentSMC X520 pin layout .zip (1305 Downloads) |
Follow us on