10/10/2022 3:59 PM | |
Joined: 6/18/2021 Last visit: 9/16/2024 Posts: 27 Rating: (0) |
Hi..hello everyone Kindly plz help me to program logo PLC Actually I have logo 24RCE PLC with RTD module in this I have connected PT100 sensor Soo..... Actually I nead to control 6 stage digital output, base on PT100 sensor temp setpoint, and the setpoint should be single eg. SP : 20 degree And dedband should be 2 degree , and within this my all output should be on within this 2 degree temp dedband Eg. 2 Degree dead band = 100% 1) 16 % stage 1 2) 33 % stage 2 3) 50 % stage 3 4) 66 % stage 4 5) 83 % stage 5 6) 100 % stage 6 Base on temp output should be on independently with 2 degree of dead band ... Kindly plz help Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/11/2022 03:57:12New subject after splitting |
|
Follow us on