2/15/2024 10:41 AM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981) |
if you have the correct TIA Step7 version installed then you can Upload it |
2/15/2024 10:53 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating: (0) |
so there's no way to download a decompiled project from there? |
2/20/2024 10:59 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating: (0) |
thank you :) is there a way to determine the correct tia portal version I need to use? |
2/20/2024 11:08 AM | |
Joined: 5/12/2006 Last visit: 5/1/2024 Posts: 22243 Rating: (2981)
|
afaik no, you can use the latest and try, they will then say if is not possible and which version is need |
4/16/2024 9:09 AM | |
Joined: 2/15/2024 Last visit: 4/18/2024 Posts: 29 Rating: (0) |
Thank you!!! |
This contribution was helpful to1 thankful Users |
Follow us on