4/20/2020 2:53 PM | |
Posts: 4 Rating: (0) |
Hi, Someone can help me please. How can'I connecting two CPUs redondance (416-5 H PN/DP) with optical fiber in SEMATIC manager. May be the synchronisation modules are intergrated in CPUs (IF1 and IF2). ------------------------------------------------------------------------------------------ |
Last edited by: Milo66 at: 04/20/2020 15:11:53Last edited by: Jen_Moderator at: 04/21/2020 09:29:42New subject after splitting |
|
4/20/2020 3:28 PM | |
Joined: 9/27/2006 Last visit: 5/14/2024 Posts: 12257 Rating: (2668)
|
Hello Milo; Could you explain your problem with more details? Do you mean that in your HWConfig editor you cannot see the synchronization cables? That is normal, if you are introducing a redundant pair of S7-400H CPUs in your configuration then it is understood that the synch module cables are present and connected on the physical installation. You would not be able to see and connect them in Step 7. Is your problem different? See if the contents of this manual on synchronization modules can give you an answer: https://support.industry.siemens.com/cs/ww/en/view/109779483 Come back to us if you do not find a solution in such a document. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 04/20/2020 15:40:07Last edited by: dchartier at: 04/20/2020 15:46:24 |
|
Follow us on