工业业务领域支持中心
Technical Forum
6/29/2011 5:33 PM | |
Posts: 22 Rating: (0) |
Ididthe communication settings of Pac3200from manual. IP:192.168.1.10 Subnet:255.255.255.0 Gateway:192.168.1.1 Protocol:Modbus TCP I did everything that described of link, but i could not carry out that application. http://support.automation.siemens.com/WW/view/en/50428682 I can't ping ip address of PC3200 through the HMI or PC. What should i do? Best Regards... |
7/1/2011 2:59 PM | |
Posts: 22 Rating: (0) |
Hello all, I did everything that described at the link http://support.automation.siemens.com/WW/view/en/37450303 but i couldn't carry out that application. I can't find where I did error. Please help... Best Regards... |
7/11/2011 8:40 AM | |
Posts: 50 Rating: (6)
|
Hello, Please control your communication protocol, menue point 21.6. Modbus TCP or SEAbus TCP? Do you use the actually firmware V2.2. LINK: http://support.automation.siemens.com/WW/view/de/31674577 Do you have the same problem with the SENTRON powerconfig Software V2.2? LINK: http://support.automation.siemens.com/WW/view/en/50241697 Deactivate the installed security-/ firewall software (Cat Client / virus scanner, windows firewall, etc…..) which can limit your network service. |
Follow us on