1/23/2023 10:46 PM | |
Joined: 1/23/2023 Last visit: 1/30/2023 Posts: 2 Rating: (0) |
PLEASE ANY SOLUTION FOR THIS PROBLMS TIA PORTAIL V16/17/18 the installation medium is not available. please insert a dvd or check the network connection MY pc dell LATITUDE 5320 I7-1165G7 32 GB RAM 512 GB SSD WINDOWS 11 PRO 64BIT ------------------------------------------------------------------------------------------ |
Last edited by: nassim_nb at: 01/23/2023 23:30:56Last edited by: Jen_Moderator at: 01/24/2023 10:08:43New subject after splitting |
|
1/24/2023 10:27 AM | |
Joined: 3/30/2020 Last visit: 5/19/2024 Posts: 4513 Rating: (943)
|
Assuming that Mr. Stefan is correct, there is software that can keep the ISO mounted through a restart (persistent). |
Last edited by: qwazee at: 01/24/2023 10:29:53** This is not an endorsement. Use of 3rd party software is at your own risk. Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
6/29/2023 7:27 AM | |
Joined: 6/7/2023 Last visit: 6/30/2023 Posts: 5 Rating: (0) |
I have the same problem and I downloaded from siemens support webpage. |
6/29/2023 8:26 AM | |
Joined: 1/21/2013 Last visit: 5/18/2024 Posts: 2795 Rating: (452)
|
Hi maherotti, If you received this message after the installer asked you to restart your PC, you probably received this message because you mounted the downloaded iso file using a feature built into Windows. This feature does not remount the file on reboot. So simply remount the iso file by double-clicking its icon and the installer should be able to find the virtual drive again. If you get this message when rebooting after the installer has finished, something went wrong when the autostart entry should have been deleted. You need to delete it yourself. See ElonksuM_SN_BN's instructions. Kind regards |
Follow us on