6/23/2022 5:34 PM | |
Joined: 4/28/2015 Last visit: 6/29/2022 Posts: 2 Rating: (0) |
Hello One of my customer want to control the 3RW55 soft starter through three modes as below 1) Control through High feature Profinet port 2) Control through panel push button stations ( On / OFF ) 3) Control through Start / Stop pushbutton available in the High feature HMI. How to achieve the above operating modes and select between these modes. Kindly help me to answer my customer query. Regards Murugaraj S Siemens Limited India ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/24/2022 09:27:48New subject after splitting |
|
6/24/2022 10:17 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873) |
Hello, Exact application to suit your requirements are not found, but you can refer below examples, which may help you. 3RW55 soft starter - Reading and writing data sets with S7-1500 and HMI connection Sample project SIRIUS Soft Starter 3RW5 PCS 7 Library V9.0 SP2 Update 1 S7-1500 with 3RW5 Soft Starter: Reading and writing data sets with HMI over MODBUS TCP/RTU |
Follow us on