10/7/2024 5:56 PM | |
Joined: 6/18/2021 Last visit: 10/7/2024 Posts: 29 Rating: (0) |
Dear LOGO Family, Today, I am facing an issue with the LOGO PLC. When I connected the LOGO PLC to my laptop through a LAN cable, I am able to access the LOGO webpage. However, when I connected the LOGO PLC to my Wi-Fi router, I am unable to open the LOGO webpage through my mobile phone after entering the LOGO PLC's IP address. All IP addresses and access control settings assigned to the controller are attached in the zip file. Kindly please assist. Soo that what IP I should set soo that I should able to see LOGO webpages on my mobile phone Thank you, AttachmentLOGO PLC IP settings 10-07-2024 21.42.pdf (1 Downloads) |
Follow us on