7/29/2021 1:16 PM | |
Joined: 12/18/2014 Last visit: 10/8/2024 Posts: 33906 Rating: (4216)
|
Have you a link to the manual or can you upload the manual? |
7/29/2021 1:47 PM | |
Joined: 7/30/2018 Last visit: 6/18/2024 Posts: 13 Rating: (0) |
See enclosed SMA Modbus manual. Some additional notes: You mention that 16 bit is +/-32767 (= signed16) which suggests I can only read up to 327,67 Volt. Is there a way to use it as U16 -> 0-65535 ? --> up to 655,35 Volt ? I still get no data, tried to read 30777 as this reads a value always below 1.000 (Watts per phase) so no risk of overflow of value 32767. Still no data ... Is there an alternative way to see if there is any data in variable memory at all ? AttachmentSMA_Modbus-TI-en-15.pdf (722 Downloads) |
7/29/2021 2:05 PM | |
Joined: 12/18/2014 Last visit: 10/8/2024 Posts: 33906 Rating: (4216)
|
The knows S16 values by the analog values. |
Follow us on