2/24/2025 9:46 AM | |
Joined: 5/6/2022 Last visit: 9/15/2025 Posts: 589 Rating:
|
Hi rlc.carmignani, In this case, I would recommend you to follow the procedure below to try to solve the problem with the Comfort Panel MiniWeb server: - Reset the panel to factory settings: "How do you do a SIMATIC HMI operating system update (firmware update, OS update) on operator panels or perform a "Reset to factory settings"?" - Delete the IM folder of the affected project: "How do I delete the IM folder of my TIA Portal project?" - Open the project through TIA and upload it back to the HMI panel. What is the result? Additionally, as an alternative I propose, you may be interested in sharing the files stored on the USB inserted in the panel with a shared network folder. For this, you can follow the following documentation: "Integration of HMI operator panels in TCP/IP networks and access to a NAS hard disk or a Windows shared folder and data exchange using "SIMATIC Option+ Manager" Best regards!
|
If this Information really helps, you could use the Rate function |
|
Follow us on