6/25/2010 6:12 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, general there are two ways: 1.) Using the fixed process image of the BackgroundTask When the I/O Adresses of the IM is in the space 0 .. 63 then you can access the I/O directly in program with the syntax %In.x or %Qn.x (n=byteadress, x=bitadress). 2.) Via direct access with I/O variables This is the way you describe in you post an works for adresses >=64. Detailed Informations are documented in Capter 5.3 in the following Document: SIMOTION SIMOTION SCOUT SIMOTION ST Structured Text Hope this helps. Regards Christoph |
Last edited by: ChristophD at: 6/25/2010 6:12 AM |
|
Follow us on