12/19/2012 9:56 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating:
|
Hello, Lot's of guestions in one post Some answers. You don't have to stop the PLC to download or upload (300 and 400 CPU) The older 300 had a switch position RUN-P to be able to program in run. If you want you can stop/restart the plc with step7 (operating mode) SDB's contain the hardware information that was build with the Hardware Configuration. You will find some good examples here Training Module DownloadRegards, Marcjan |
Last edited by: Marcjan at: 12/19/2012 9:58 AMProblem solved? |
|
This contribution was helpful to
1 thankful Users |
12/20/2012 7:13 AM | |
Posts: 1064 Rating:
|
The only time you need to put in stop mode is you are changing the hardware configuration |
Follow us on