8/28/2014 8:43 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating: (2675) |
Hello mohagan; Welcome to the forum. This document on the Diris 40 states that the protocol supported by the Ethernet module of the Diris 40 is Modbus/TCP: diris a40/a41 ethernet - Socomec Group Siemens offers support for Modbus/TCP through specialized function blocks under the designation Open Modbus TCP. Have a look at the Siemens IT4Industy webpages on the different products offered: S7 OpenModbus/TCP - IT4Industry - Siemens You would need to download the project and documentation for the "Open Modbus TCP for PN CPUs", if you were planning to use the onboard TCP/IP connection of the CPU. The license for theseblocks will need to be purchased eventually, as the missing license generates constant error messages in the CPU, ant a client does not appreciate the diagnostic LEDs of a CPU to be active. But the download will be fully functionnal to test the installation and communications with the Diris 40. Siemens also provides a free-downloadable tool to make your life easier when configuring the Modbus/TCP exchanges: Wizard for creating connection data for Modbus TCP communication. (Modbus TCP Wizard) Hope this helps, Daniel Chartier |
8/29/2014 1:03 PM | |
Posts: 9 Rating: (0) |
thanks for your reply i have a problem with download from it4industry??? |
8/29/2014 3:58 PM | |
Posts: 9 Rating: (0) |
hello dchartier thanks you very much i register again with new email and password it work now i'have to complete my programme and i'll see! thanks |
8/30/2014 8:38 AM | |
Joined: 9/1/2005 Last visit: 7/9/2024 Posts: 4101 Rating: (194) |
new question published by mohagan@2013is split to a seperate thread with the subject connect diris a40 - problem with mapping register adress. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on