1/27/2017 9:39 AM | |
Posts: 1368 Rating:
|
Hello, in TIA you configure your PLC and ET200SP. In ET200SP you add the CM AS-I Master and create a new AS-I Network. In HW catalogue, you also find AS-I Slave, which you can add to the AS-I network. Also there, you define AS-I Adresses to each slave which must be the same as in "real" AS-I Slave. Every Slave becomes an address area in S7-1500. The manual of AS-I CM is here: For AS-I Diagnostic, there is a configuration example in SIOS: it is not difficult:-) |
1/28/2017 4:24 AM | |
Posts: 5 Rating:
|
thank you |
Follow us on