10/11/2015 7:27 PM | |||||||||
Joined: 5/12/2006 Last visit: 8/8/2024 Posts: 22338 Rating: (3003) |
Old links, not ther best idea or?
|
||||||||
This contribution was helpful to1 thankful Users |
10/11/2015 7:34 PM | |
Posts: 784 Rating: (52) |
Hello, 1-Is it possible to install this tool alone without installing TIA in the PC? 2-Is it suitable for V11,12,13 to perform the all tasks of the tool? |
10/11/2015 7:46 PM | |
Joined: 5/12/2006 Last visit: 8/8/2024 Posts: 22338 Rating: (3003) |
Regards Christoph |
Last edited by: ChristophD at: 10/11/2015 7:51:34 PM |
|
This contribution was helpful to1 thankful Users |
10/11/2015 7:53 PM | |
Posts: 784 Rating: (52) |
Hello, To perform these tasks:
in a simatic controller programmed with V11 ,V12 or V13 |
10/11/2015 8:04 PM | |
Joined: 5/12/2006 Last visit: 8/8/2024 Posts: 22338 Rating: (3003) |
Hello, yes this task possible indepent from which TIA Version the PLC is loaded/configured. Regards Christoph |
This contribution was helpful to1 thankful Users |
10/11/2015 8:10 PM | |
Posts: 784 Rating: (52) |
Hello, 1-Why this tool not extend to include Simatic controller 300 and 400 which programmed by TIA? 2-Why the program uploading is not supported by this tool? |
10/11/2015 8:14 PM | |
Joined: 5/12/2006 Last visit: 8/8/2024 Posts: 22338 Rating: (3003) |
Hi,
The prograsm download with the Automation Tool is simple a download of the CardData which you create with TIA Portal. Regards |
This contribution was helpful to1 thankful Users |
10/11/2015 8:22 PM | |
Posts: 784 Rating: (52) |
Hello, Is automation tool can
|
10/11/2015 8:29 PM | |
Joined: 5/12/2006 Last visit: 8/8/2024 Posts: 22338 Rating: (3003) |
Hi, no the Tool downloaded the MemoryCard Data which you create with TIA Portal to the PLC! You create the CardData for the PLC offline in TIA. This data now you can download with the tool to the PLC. Regards |
Last edited by: ChristophD at: 10/11/2015 8:33:25 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on