11/12/2015 2:00 PM | |
Posts: 1529 Rating:
|
It's installed but it does not work. I uninstalled it and re-installed Startdrive_optional_sp1. Attached is the Log File. The line that concerns me is 20:34:55 |ERROR AdsWorkerForeignExe::GetInstallResult(): - -777: FILE_NOT_FOUND. Please check the corresponding log file for more detailed information No idea which log file it is referring to. I should note that my TIA is configured for both English and Chinese, if that makes a difference. AttachmentStartdrive_option_sp1 log file.txt (277 Downloads) |
11/13/2015 1:27 AM | |
Posts: 1529 Rating:
|
Hope this is the correct log file. I do not have the remove V47.cmd file in my /bin directory (or any .cmd files, only dll's). First time I've had an update problem. I'm re-downloading the update file in case it was somehow corrupted. AttachmentSIA_STARTDRIVE_OPTIONAL_V13@15-11-13_07-30-28 - Long.txt (242 Downloads) |
11/13/2015 4:48 AM | |
Joined: 5/12/2006 Last visit: 8/14/2024 Posts: 22343 Rating:
|
Hello, i have extrac the file from my Installation. Try to copy the file to the path "C:\Program Files (x86)\Siemens\Automation\Portal V13\Bin\" an try a reinstall or uninstall and show if it works. Regards Christoph Attachmentdelete_HSP_47.zip (289 Downloads) |
This contribution was helpful to
1 thankful Users |
3/8/2017 9:43 PM | |
Posts: 1 Rating:
|
Hi Jeff, I have the same problem and will try to install Update 2. Did you have issue with the end result? |
Follow us on