10/8/2016 9:25 AM | |
Posts: 8 Rating:
|
Thanks for the reply. So what, basically I should use (S) and (R) instead if I have multiple inputs that trigger one output? |
10/9/2016 4:12 PM | |
Posts: 30 Rating:
|
Jeff and Mindware are right. If you use coil/output in multiple place, it may lead to confusion as well as malfunction in your logic. It is better to use output in a single network and implement all logic to it rather than distributing your program logic wise. If you still needs to set state of output from single/multiple conditions in other networks, the better idea is to use memory bit (either M or DBX) which defines the state of logic in other networks. Use this memory bit in the condition of the subject output. In other words, the memory bit that define the logic state in other networks, indicates that this bit is being used in some other single or multiple places, thus, reducing confusion and giving more flexibility and reliability in the program.
AttachmentConveyor.pdf (133 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on