6/12/2017 12:54 PM | |
Joined: 3/30/2017 Last visit: 12/27/2022 Posts: 3 Rating:
|
Hi, please help us configuring a hart field device via hart analogue card the analogue card we are using is siemens AI8x16Bit HART card(6ES7 331 -7TF01-0AB0 V3.x) following are the steps we did so far 1) insert an IM 153-2 (6ES7 153-2BA02-0XB0) in to an already existing Profibus DP Master System( attachment) 2) insert the HART analogue card in to slot 4 of the IM and enable the HART mode 3)add the field device to the channels 4) connect the field device (in this case VEGA DIFF 65) in to the first channel of the analogue card. after connecting the filed device to channel 0 of the analogue card, we tried to double click the channel in the hardware config . it opened up a new window where it asked to assign a device. selected the VEGA DIF Revision 7.0 and when we click the device identification button , it gives an error-'action failed: the device was not found or couldnot be identified.OM:parameter invalid.' please see the attachment. at this stage we dont know what else to do to move forward. we checked the EDD file in the device integration manager of the PDM and the file is the latest one for the device. we are using PDM 8.2 please give us the steps that are required to configure the hart device so that we can communicate via PDM. thank you very much Attachmentvega error.zip (246 Downloads) |
6/13/2017 6:42 AM | |
Joined: 3/30/2017 Last visit: 12/27/2022 Posts: 3 Rating:
|
thank you. hardware download was done. |
Follow us on