12/7/2016 9:54 AM | |
Posts: 72 Rating: (1) |
Hello, I have recently worked with TIA Portal V13, Startdrive and Siemen’s G120 drive. Presently, I want to do similar steps with TIA Portal V13, Startdrive and Siemen’s DCM drive (6RA8013-6DV62-0AA0-Z) via Profinet (see also attachment), but I found there some problems. I have downloaded GSD file from:https://support.industry.siemens.com/cs/document/98207877/sinamics-s150-g130-g150-gm150-gl150-sl150-sm120-dcm-dcp%3A-profinet-gsd-file?dti=0&lc=en-WW. ->GSD_Profinet_DCM32.ZIP (32 KB)( 32 KB ) I have installed it and now in Tia Portal are many new elements (see attachment).
I'm not using PLC yet. Can I control DC without PLC controller via Profinet and Startdrive in TIA Portal? I am counting on your help. Regards, Adam |
Last edited by: AdasK at: 12/7/2016 9:58:43 AM |
|
12/7/2016 10:26 AM | |
Posts: 72 Rating: (1) |
OK, I understand. Thank you very much for you answer. Regards, Adam |
12/7/2016 11:46 AM | |
Joined: 5/12/2006 Last visit: 7/16/2024 Posts: 22316 Rating: (2998) |
Hi, which PLC you use and which engineering software? Regards Christoph |
Follow us on