9/5/2008 10:05 AM | |
Joined: 1/24/2008 Last visit: 11/13/2021 Posts: 7 Rating: (3) |
I have recently added a CP 443-1 to an existing project. I configured the card in the hardware configuration and downloaded the configuration. But when I inserted the new CP 443-1, all the LED's on the CPU, and I mean ALL the LED's started fashing together. I then thought that maybe the slot in the UR is faulty so I moved the card to the next available slot. It stil does the same by lighting up all the LED's. Also the 5V LED on the PS 407 4A flashes green. I then REMOVED the CP 443-5 Basic card and and left the CP 443-1 in,then the CPU goes into RUN mode and PS 407 4A 5V LED goes solid green. All looks fine now but I still cant get communication with CP 443-1 and PG. Can I configure both a CP 443-5 Basic and CP 443-1 with CPU 414-2DP? Also, can I update FIRMWARE of CPU 414-2DP with only MPI cable? Kind regards, Simatic Junky AttachmentHardware Config.pdf (77 Downloads) |
Follow us on