4/25/2019 11:17 AM | |
Posts: 11 Rating: (0) |
hey guys, quick question. Is there a way to distinguish supply voltage missing from short circuit. is this iven possible at all? I Use s7-1511-1PN the module that i want to detect the short circuit on is 6ES7 522-1BH01-0AB0 Tia portal 15.1 is there some kind of block that i can use that lets me see what the exact error is instead of showing me that there is an error but not which. In attachment you see the data i recieve between short circuit/ voltage supply missing and no error. the numbers don't change a bit between short circuit and supplyvoltage missing. the only thing that does change is the channel number. So is there a way to distinguish short circuit and other errors? thanks in advance AttachmentAll values.zip (47 Downloads) |
4/25/2019 1:24 PM | |
Joined: 8/31/2005 Last visit: 6/14/2024 Posts: 2198 Rating: (328) |
Hace a look on the SITOP selectivity module: https://support.industry.siemens.com/cs/ww/en/view/108989004 Maybe this can be a solution for you. |
|
|
Follow us on