4/24/2023 9:04 AM | |
Joined: 4/21/2023 Last visit: 6/18/2024 Posts: 4 Rating: (0) |
Dear experts I've encountered a problem with a S7-1510SP. According to the diagnostic buffer the CPU rebooted at 3:39AM and restarted on his own. But I can't figure out why the CPU state changed from RUN to OFF mode. What could be the cause of this state change? Thanks in advance. Regards Diagnostics buffer of the module [CPU 1510SP-1 PN] AttachmentDiagnostic_buffer.txt (471 Downloads) |
Last edited by: Jen_Moderator at: 04/25/2023 05:29:26Diagnostic buffer added as .txt file. |
|
4/24/2023 9:22 AM | |
Joined: 5/6/2022 Last visit: 8/7/2024 Posts: 439 Rating: (86) |
Hi KilianDB, As you say, the event with reference "Event ID: 16# 02:400C" that appears in the diagnostic data of your CPU, simply indicates that the CPU has gone from START to RUN state. In order to find out possible causes of the behavior you are experiencing, and in order to gather as much information as possible, could you please attach the complete diagnostic buffer in .txt format? However, this kind of behavior can also be caused by a corruption of the internal FW of the CPU. Therefore, I recommend you to upgrade the FW of your CPU (6ES7 510-1DJ01-0AB0) to the latest available version which you can download from the following link: "Firmware upgrade for 1510SP-1 PN CPU" Best regards! |
If this Information really helps, you could use the Rate function |
|
4/24/2023 10:00 AM | |
Joined: 4/21/2023 Last visit: 6/18/2024 Posts: 4 Rating: (0) |
I'll attach a printout off the diagnostic buffer. It seems in event 5 Event ID: 16# 02:4002 that there's a sudden shutdown. Thanks for the info about the firmware upgrade. Best regards AttachmentPLC_Diagnostics.txt (390 Downloads) |
4/24/2023 1:22 PM | |
Joined: 4/21/2023 Last visit: 6/18/2024 Posts: 4 Rating: (0) |
We're using a Sitop PSU300S. |
4/26/2023 6:13 AM | |
Joined: 4/21/2023 Last visit: 6/18/2024 Posts: 4 Rating: (0) |
Thanks for the advice, I'll try to monitor the supply voltage. |
Follow us on