7/28/2021 3:09 PM | |
Posts: 198 Rating:
|
Hello Zankkar, Firstly, ET200SP bundle 6ES7155-6BA01-0CN0 contains the following components:
The server module closes the backplane bus of the ET200SP. Hence, you need to ensure the server module is configured and present both physically and in your hardware configuration. You need to configure and assign parameters to the server module in the configuration software. Place the server module on the last slot of the configuration. If there are 64 I/O modules, the server module is plugged in slot 65. Are you facing any compilation / consistency check issues while saving/compiling the hardware configuration? The module driver can occur because of multiple reasons:
I've also attached the ET200SP manual for your reference. Hope this helps Attachmentet200sp_im_155_6_dp_hf_manual_en-US_en-US.pdf (343 Downloads) |
Last edited by: TechnoBlaze at: 07/28/2021 15:11:49Last edited by: Jen_Moderator at: 07/29/2021 06:00:25Optimized link. |
|
7/29/2021 3:47 PM | |
Joined: 2/7/2020 Last visit: 6/27/2024 Posts: 101 Rating:
|
Thank you for details. 1. I am not able to find IM "6ES7155-6BU01-0CN0" in Release module list. All other modules available in list. Please suggest 2. Server modules added at end 6ES7193-6PA00-0AA0 I am not facing any issue while compiling. Which parameters need to configure and assign to the server module in the configuration software. Please suggest- I have not done any setting. Thank you for mentioning 3. Diagnostics are enabled. Thank you again, Zankkar
|
Last edited by: Zankkar at: 07/29/2021 15:52:06Please suggest |
|
8/19/2021 7:01 AM | |
Joined: 2/7/2020 Last visit: 6/27/2024 Posts: 101 Rating:
|
Hi, If any one is already aware this kind of problem, please suggest. @TechnoBlaze, Hi, If you are having GSD file, it would be really helpful, if you can share Thank you
|
Follow us on