6/26/2015 10:47 PM | |
Joined: 9/27/2006 Last visit: 7/14/2024 Posts: 12268 Rating: (2675) |
Hello Koenraad; When you work with Siemens documentation, it is sometimes difficult to determine which modules do not support certain functions, because they are not mentioned In the "supported modules" tables. If it not explicitly mentioned, the function is not supported. You have to learn and live with this mindset. In the case of routing functions and a DP/DP coupler, you can see (with a bit of search) that it is not included in any of the routing list of this FAQ: Which modules support the "S7 Routing" function in S7 subnets? So we should deduce that it will not help in your project, at least not in the way you are asking. Hope this helps, Daniel Chartier |
6/29/2015 4:41 PM | |
Posts: 11 Rating: (0) |
Thank you for this information. I did not realize that this process was called routing, so at least i learned something. |
Follow us on