10/16/2007 1:53 AM | |
Joined: 5/25/2006 Last visit: 3/21/2024 Posts: 28 Rating: (2) |
Dear friends, I have a problem when I try to download the hardware to a CPU 416-3 DP (6ES7 416-3XR05-0AB0). The problem just appear when I add a IM 153-1 on the Profibus. I'm able to compile but can't download . If there is no IM 153-1 just PS, CPU and CP 443-1 I can compile and download without problems. I just upgrade the firmware, thought that could fix my problem but no. The only way to work with the IM153-1 and the CPU is changing the CPU type to 6ES7 416-3XL04-0AB0, wiht this, I only get a warning message when download the hardware (because the differences beetween CPU types) but there's no more problems . I can't realize what could be the problem. Hope that someone can help me. I'm attaching the diagnostic buffer of the PLC. AttachmentDiagnose.zip (298 Downloads) |
10/18/2007 1:49 PM | |||||
Posts: 70 Rating: (3) |
Hi - check the version of your Step7 -you need 5.4 SP2 or higher. From the manual : http://support.automation.siemens.com/WW/view/en/23904550 it is stated that : 6ES7416-3XR05-0AB0 requires :
You can find the newest SP here : http://support.automation.siemens.com/WW/view/en/25602738 Happy downloading Søren |
||||
10/18/2007 11:52 PM | |
Joined: 5/19/2006 Last visit: 6/20/2024 Posts: 548 Rating: (107)
|
Well, I attached a screen-shoot from the manual you refer and it stated STEP7 v5.3 SP2 with hw updates. BTW the latest SP for STEP7 is SP3 for v5.4 Somehow the SP3download link got lost (I just downloaded 2 days ago) Dec PS David, What happens when you download the HWConfig? Attachment3XR05.zip (281 Downloads) |
Last edited by: Dec at: 19.10.2007 01:15Last edited by: Dec at: 19.10.2007 01:12Last edited by: Dec at: 19.10.2007 00:14 |
|
10/19/2007 10:00 AM | |
Posts: 70 Rating: (3) |
Hi Dec - I think you are right, but I copied the text from the document....anyhow my expirience shows that if you do not have te newest sw with the new hw you are bound to face throubles, especially if you use the new advanced ethernet cards aswell. I got my 5.4 SP3 from the subsribtion service at Siemens a couple of weeks ago - have not seen an online link yet. btw : It is OK to use the v4 cpu in thehw configuration and then insert the new CPU - only thing though is that you'll get a fault indication on the front of the CPU /søren |
6/20/2016 4:20 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
New question published by HammaMiny is split to a separate thread with the subject Failed to go to run mode after a hardware change. Best regards |
Follow us on