10/6/2015 1:37 PM | |
Posts: 5 Rating: (0) |
hi mr i suggest you chenge of backplane of cuvc card becuse all of ct connected this card . best regard |
10/7/2015 3:08 PM | |
Posts: 2 Rating: (0) |
The CT are directly connected to the IVI interface card, not on CUVC |
11/10/2015 8:25 PM | |
Posts: 94 Rating: (2) |
Is F011 is the only alarm appeared if there are another alarms like f006 f025 may be it is dc power fault |
7/22/2018 7:02 AM | |
Posts: 1 Rating: (0) |
same problem encounterred. anybody here solve this problem? |
Follow us on