7/7/2014 12:14 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating:
|
Hi! I suggest you to take a lool at SNMP diagnostics. Here is whatmanualsaid: The SNMP OPC server makes available the SNMP information from TCP/IP networks on the IOPC interface with SNMP (Simple Network Management Protocol). With the aid of the SNMP OPC server, any OPC client systems (such as WinCC) can now access diagnostic and parameter data of SNMP-compliant components. Non SNMP-compliant components can also be included in the plant visualization using their IP addresses. This allows, for example not only simple device diagnostics but also detailed information such as redundant network structures or network load distributions of entire TCP/IP networks to be displayed. Here is alink(SNMP OPC Server) As for general fiber optic initial diagnostics, look at specifical devices such asFlukeor similar. Hope it helps. For detailed information, more experienced colleagues will suggest something else) |
Follow us on